Posted by Sichao CHENabout 4 years ago
HVU2- Large diameter on profis engineering
Hello
Are anchors HVU2 M24 and plus on profis engineering or not yet? If not, do you know when it will happen?
Thank you for your help.
1 Reply
Posted by Ram Neupaneabout 4 years ago
Hi Sichao,
Thanks for your question.
The current version of PROFIS Engineering is 3.0.58, which includes HVU2 up to M24 in Australia. It, however, doesn’t include the HVU2 capsule above M24 at the moment, which is because the product is not available in Australia. If you are designing for overseas projects where HVU2 capsule above M24 is available, you can design it by changing the region from the setting tab. HVU2 with M27 and M30 anchors are covered by the ETA approval (ETA-16/0515) and popular in Europe (e.g. the United Kingdom).
Cheers!
Ram